4/20/2012 10:10 AM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
Dear friends, I totally agreed with "CS Moderator" here.It is not proper to ask people suppress their feelings of appreciation regarding a post.
For divergence of main topic ,we simply ask the moderators to split this part.It is an open discussion and each member write his/her idea. Best regards, Hamid Hosseini |
4/20/2012 10:54 AM | |
Posts: 270 Rating: (53) |
Yeah, I reported my previous post to moderators with that information. And since that wouldn't really be worth writing alone, there's one more think about rating - I think, people would rate more if it was easier. This might sound ridiculously funny, but the user experience is somewhat very delicate science when it comes to tuning website right (not that I would fully understand those things, but having some experience with websites from creation point of view, I at least know that there's plenty DOs and DON'Ts about it etc.) So what I mean by "it being more easy", well, the fact that you have to click on one extra button, everything disappears except the rating screen, then you choose one and then it has to redirect you back, users would not use something for much much less. Since easies way to describe it is with a picture, I quickly compiled one in ms pain(t), so excuse the quality. I did circle two things in red -area a: once user would rate the post, that part would "disappear", so the only ratings would remain; area b: since thank wouldn't most likely fit in the top, it would have to be moved down (when I think about it, I see that as a logic move, I'm surely not gonna thank a user before I read the post he wrote, but perhaps then even the rating stars should be at the bottom too). |
Last edited by: MM1234 at: 4/20/2012 10:56 AMtypos |
|
4/20/2012 4:11 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
I think moderator told here that they are going to change this rating method and going to implement Overlay for rating in same page only
|
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
4/20/2012 4:57 PM | |
Joined: 1/28/2009 Last visit: 9/10/2024 Posts: 6849 Rating: (1365) |
This is my question: "This could be published in announcement conference". Information provided in the forum, when you face a problem and seeking for solution, then you understand "Rule" changes. |
4/20/2012 5:01 PM | |
Joined: 7/8/2009 Last visit: 8/5/2024 Posts: 1976 Rating: (477) |
I think they will announce when they will Implement the same This was just a suggestion by some user and Moderator given reply for that May be this issue discussed in Past.. or may be in German Forum Just be cool and have fun Regards Devesh Vithani |
I dont Like people driving Fast, thats the reason I overtake them ;) |
|
This contribution was helpful to1 thankful Users |
4/23/2012 10:04 AM | |
Posts: 270 Rating: (53) |
Well, that's pretty good then, I actualy even recall reading that post back then, gosh... It's always the same, me living the life like in Memento... ;]] |
Last edited by: MM1234 at: 4/23/2012 12:04 PM |
|
Follow us on