10/22/2014 12:37 PM | |
Joined: 7/7/2010 Last visit: 5/7/2024 Posts: 14688 Rating: (2351)
|
Check the FBD block attributes regarding setting ENO automatically. Toggle and try again. |
science guy |
|
10/22/2014 5:27 PM | |
Joined: 5/27/2009 Last visit: 11/28/2019 Posts: 31 Rating: (0) |
Hi, As yo see at the attachment there's no attribute like that... How can I make it visible? Thanks A Lot...
|
10/22/2014 5:56 PM | |
Joined: 7/7/2010 Last visit: 5/7/2024 Posts: 14688 Rating: (2351)
|
My mistake. The option I was thinking of is only available for SCL in S7-1200's - to set ENO automatically or not. Maybe it is time to send a Support Requestto solve that specific problem. Back on topic though, what is it you want to solve? Do you want to use legacy step 7 in Portal, or do you want to solve problems in the ways portal was designed to be used? Either way, compromises are made. It is simply a matter of when do you stop making compromises and redesign and use Portal the way it was intended. If you choose now, perhaps you could describe the problem that you think having control over EN and ENO solves for an FBD or LAD block. |
science guy |
|
Follow us on