7/28/2011 10:36 AM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
Hello, you get the error at the panel or in WinCC V11? Wich error do you get exactly? best regards |
7/29/2011 9:13 AM | |
Posts: 150 Rating: (17) |
Sorry, I forgot to mention that the problem still persists on the second PC. |
7/29/2011 9:39 AM | |
Joined: 4/24/2006 Last visit: 4/15/2024 Posts: 8610 Rating: (1146) |
Dear Nikzitronik, Do you already have Update 2 for WinCC V11? Here you can download: Updates for STEP 7 V11 and WinCC V11 Perhaps it might help. Best regards, Wizard |
7/29/2011 9:44 AM | |
Posts: 150 Rating: (17) |
Dear Wizard, The updates are already installed but I get the same responce. |
7/29/2011 11:00 AM | |
Joined: 8/31/2010 Last visit: 4/14/2024 Posts: 1509 Rating: (221) |
Hi Nik, If u ping the IP address of your TP177B from your PG/PC, what response you get? |
Like it? Rate it! |
|
7/29/2011 6:00 PM | |
Posts: 150 Rating: (17) |
Dear Ganes10, When I ping the TP177B it responds normally I thing the responce was 128 ms. |
Follow us on