5/14/2014 3:27 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2349)
|
I had a similar problem recently and contacted Siemens Support via Support Request. V13 does not have any compatibility mode like V12 did for V11 projects. Sigh. I do not know how I was thinking V13 could open V11 and V12 and V13 and act as a native environment for the version it was working within. This would be a huge benefit to end-users as the upgrade path would leave working and installed and accepted systems/projects in the portal version currently being supported by customers/clients. Sadly, V13 only works with V13. It can upgrade a V12 to a V13 project, and lose compatibility with V12. So, if you work with others, everyone would need to upgrade to V13 or no work could be shared between projects and all projects would likely need to be upgraded to V13. However, as many have said, you can use V12 SP1 in compatible mode on V11 projects and natively for V12 projects, and V12 can coexist with V13. Hope this helps. The V13 license [supposedly]will also work for V12 on the same computer. :) |
science guy |
|
This contribution was helpful to1 thankful Users |
Follow us on