12/4/2020 6:28 AM | |
Posts: 1 Rating: (0) |
Hello I have a 6ES7 212-1AD30-0XB0 1212c AC/DC/RLY with firmware 1.02 when i try to use this PLC in the TIA Portal V15.1 i recieved a error with the indication of NO COMPATIBLE. Any sugestion that don`t represent the necesity to upgrade the firmware to v2.2? Please Help : ( Thanks |
12/4/2020 7:07 AM | |
Joined: 3/30/2020 Last visit: 4/19/2024 Posts: 4414 Rating: (924) |
Hello. The firmware of that PLC can only be upgraded with a special memory card. Consider talking to a Siemens representative to help if you do not already own such a memory card. The other option is to (also) install a lower version of TIA Portal. The best version would be TIA Portal V13 SP2, as it is a gateway when upgrading programs from earlier TIA Portal version to more current versions (like TIA Portal V15.1). Upgrading the PLC remains a good recommendation. BR |
Activities of this user is voluntary. There is no obligation or liability placed on this user. Though optional, your 'please' and 'thank you' is highly valued. |
|
12/4/2020 3:36 PM | |
Joined: 7/7/2010 Last visit: 4/19/2024 Posts: 14597 Rating: (2347)
|
Good answers have already been given as well as good suggestions and help. V13 SP2 if you are somehow required by law not to update the buggy 1.0.2 firmware to the much less buggy FW2.2. If law does not require the firmware not be updated, FW2.2 is definitely the right answer.
|
science guy |
|
Follow us on