12/8/2014 9:57 PM | |
Joined: 8/29/2014 Last visit: 3/5/2024 Posts: 14 Rating: (0) |
Pure TIA Portal basic v13 and HMI simulation in PC to real s7-1200 PLC do not work.... PG/PC settings is not available at all in PC control panel! what to do!?
------------------ New subject after splitting from TIA v12 Wincc simulation no communicates with PLCsim. |
Last edited by: Min_Moderator at: 12/9/2014 8:53 AMSplitted Last edited by: mahak at: 12/8/2014 10:00 PM |
|
This contribution was helpful to1 thankful Users |
12/9/2014 3:32 PM | |
Joined: 8/29/2014 Last visit: 3/5/2024 Posts: 14 Rating: (0) |
Thats the problem...there is no "Set PG/PC interface" at control panel of the PC TIA Portal basic v13is the only Siemens SW in this PC, maybe"Set PG/PC interface" is not installed at all with this pure TIA install!?
|
4/21/2015 5:10 PM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4775 Rating: (123) |
|
12/29/2015 9:10 AM | |
Joined: 9/1/2005 Last visit: 3/5/2024 Posts: 4097 Rating: (193) |
New question published by Microwin sp9 is split to a separate thread with the subject CPU 1214 and KTP400 Basic PN - no simulation between PLC & HMI. Best regards |
My Forum is the place to personalize your profile, |
|
12/31/2015 10:03 AM | |
Joined: 3/31/2012 Last visit: 3/18/2024 Posts: 52 Rating: (27) |
I had also the same problem, But solved by changing the setting above... Thanks APS....... |
Follow us on