6/20/2019 10:50 AM | |
Joined: 5/17/2018 Last visit: 4/15/2024 Posts: 26 Rating: (1) |
I changed Ip address and they are matching now but still having the same error. |
6/21/2019 10:36 AM | |
Joined: 5/17/2018 Last visit: 4/15/2024 Posts: 26 Rating: (1) |
Hi, I am not able to sort the problem out. My laptop is a simatic field PG, it has got 2 Local connections: Gigabit Local Connection and Intel Ethernet connection, I often use gigabit local connection to estabilish comunication with PLC siemens and the other local connection for internet and comunicate with other networks. The IPv4 for both networks with DHCP active (not selected Obtaion an IP address automatly) are: Gigabit Local connection: 192.254.3.177 Intel Ethernet Connection: 169.254.186.127 Ip addresses in Siemens: Tia portal Project PLC address~: 192.168.1.180 Plc target address: 192.168.1.180 (I have changed those, from another laptop) So at that point, using Gigabit local connection by default DHCP active Tia portal is not able to find PLC because out range, then I go to windows settings at local area connection status and select IPv4 and disable option "Obtain an IP address automatically" then active "Use the following Ip address" to IPv4: 192.1658.1.254 submask: 255.255.255.0 After changing those options, i check configuration in cmd/ipconfig, ip was changed sucessfull then I do another try to connect with Plc target, this time, it is founded but gives error. I can get ping in PLC, software detects PLC but not estabilish connection, I attempt connect in a different way, selecting bar option "Online" > Accesibles devices (scanning for devices) it founds plc device. At this options, I can not manage functions as reset to factory settings, diagnostic status, online access, etc.. Do not know what options more to do, I am completely desperate. Please, see attached the document which is included some pictures of the problem. Thanks, AttachmentDoc1.pdf (68 Downloads) |
Follow us on