9/8/2017 9:54 AM | |
Posts: 8 Rating: (0) |
Hi to all! My question consider configuring drive G120 and connecting it with PLC S7-1200. Suddenly appeared some problems. To make understanding more clear, here the list of my hardware:
Article: 6SL3210-1PE21-8AL0 3.PLC S7-1200 (CPU 1215C) 4.Panel TP1200 Comfort I was searching for the answers, and that’s my results: 1.)Configring the drive by the means of Startdrive v.4.5 SP1 The software successfully was integrated into my TIA Portal, but when I opened Add new device->Drives, there was Sinamics G120 drive family, and in a sub-folder «Control Units» were only CU240-2 control units. I wondered, that some S120 package should exist, and went for the answers to «support.industry.siemens.com». Misfortunetly, I found this: «SINAMICS Startdrive V14 S120 Option is now available for delivery. The product release is restricted. Please contact yourSIEMENS contactbefore ordering.» Without any references for downloading. 2.)Configring the drive by the means of Starter While installing this software a lot of errors appeared. Than I also went to «support.industry.siemens.com» and found this: So, as I understand there’s the only way to configure my system is through Starter sowftware, than export GSDML file, import it to TIA Portal and it’s done. Am I right? P.S.: In a Siemens PM240-2 Product announcement pdf is written that S120 CU310-2 is compartible with PM240-2 since Firmware >= v.4.7 or >= v.4.8 . And also G120 is coupled with CU240 in TIA Portal. Thanks for attention, any help is appreciated |
Last edited by: lucky_boris at: 9/8/2017 9:55:30 AMLast edited by: lucky_boris at: 9/8/2017 9:57:18 AM |
|
9/8/2017 11:39 AM | |
Posts: 8 Rating: (0) |
Here the logs. Log and Log_1 are the same thing, but after different installations (reinstalltion). OS: Windows 7 Professional SP1 x64 AttachmentLogs (Starter).zip (200 Downloads) |