11/7/2012 2:18 PM | |
Joined: 9/28/2005 Last visit: 3/12/2024 Posts: 2957 Rating: (242)
|
Hi, My advice: check if you have latest version of TIA software which must be V11+SP2+Upd5. If not, upgrade it (Updates for STEP 7 V11 SP2 and WinCC V11 SP2) and try again. If this doesn't help - please do not invent bycicle and one a support request casehere
|
Best regards, |
|
11/7/2012 3:16 PM | |
Posts: 19 Rating: (0) |
Thank you Darius, updating now. I had upd4, so ill test it soon. |
11/9/2012 7:10 AM | |
Posts: 19 Rating: (0) |
I have to reinstall windows first . Serveral programs that are not approved for Windows 7 SP1 are/were installed on your PG/PC. A small list: - MicroWin - S7-PLCSIM - S7-PCT - S7-GRAPH - S7-SCL STEP 7 and the combination of Step7 V5.5 (without SP) in combination with WinCC flexible Version 2008 SP3 The list of allowed combinations can be found here: http://support.automation.siemens.com/WW/view/en/18734363 I recommend you to reset your PG to a restore point or to format the hard disk. The incompatible software packages have damaged your TIA Portal installation in way that is not repairable. |
This contribution was helpful to1 thankful Users |
Follow us on