12/16/2011 3:13 PM | |
Joined: 9/23/2005 Last visit: 9/19/2024 Posts: 4347 Rating: (1446)
|
Hi, Just a note: The SP2 for STEP 7 V11 is already available in link http://support.automation.siemens.com/BR/view/en/56750498 (just INTRANET Siemens). I suppose that will be also available soon for all. |
Denilson Pegaia |
|
12/16/2011 7:54 PM | |
Posts: 68 Rating: (0) |
And this SP has 64 bit support ? |
12/20/2011 9:04 PM | |
Joined: 3/21/2006 Last visit: 9/10/2024 Posts: 10228 Rating: (1181) |
Forget about free of charge. best regards, Hristo Mihalev |
12/21/2011 10:47 AM | |
Joined: 8/31/2010 Last visit: 9/24/2024 Posts: 1521 Rating: (227) |
If you have installed the STEP 7 Basic v11 with Single License in a 32-bit OS as of now, then the downloaded SP2 of STEP 7 Basic v11 should be sufficient to make your license as a Floating License. (yes at free of cost) If you want to install STEP 7 Basic v11 in Windows 7 64-bit OS then the download will not be helpful and you can buy the STEP 7 Basic v11 SP2 Trial Software which you can install in Windows 7 64-bit OS. (the existing license can be used in Win 7 64-bit OS) For more details check here - Service Pack 2 for STEP 7 V11 Released for Delivery Change of the License Keys with STEP 7 Basic
Customers who wish to upgrade an existing STEP 7 Basic V11 32-Bit installation to SP2, require only the SP2 (e.g. Trial version). The existing License Key can continue to be used.. For a new installation (e.g. on Windows 7 64-bit operating systems), STEP 7 Basic V11 customers require the STEP 7 Basic V11 Single -> Floating License update (order no. 6ES7822-0AA01-0YC5). |
Like it? Rate it! |
|
12/27/2011 11:00 AM | |
Posts: 8 Rating: (0) |
Does anybody know when WinCC and Safety will be released for 64 bit? |
Follow us on