10/31/2014 8:52 PM | |
Joined: 7/7/2010 Last visit: 4/25/2024 Posts: 14629 Rating: (2349)
|
Your list is missing *all* DC/DC/RLY options which is where you should find your PLC part #. There should be 3 of the DC/DC/RLY options listed in the s7-1212 group. Your image shows 0. Try this as a test. Change the default portal language to English or German (whichever you can read better). Check your list again. If it is the same, submit a Support Requestto alert Siemens of the problem. |
science guy |
|
4/25/2018 5:22 AM | |
Joined: 11/23/2012 Last visit: 10/20/2020 Posts: 6 Rating: (0) |
I am trying to add an additional Output module to a machine to expand it's capabilities. However, I cannot locate a suitable HSP file it seems for the new module. The TIA 'device catalog' lists the module but only up to v2.0. The new unit I am trying to fit is a later version. New Module is 222-1BF32-0XB0. v3/4 I have updated the TIa to v13 SP1 V9. I have downloaded the latest Support package. There does not seem to be any suitable Output software file in the HSP list of the support package IN any case I've loaded up everything into the TIA that I can. Can you help please? AttachmentOutputModuleProblemSupport.docx (33 Downloads) |
4/25/2018 6:24 AM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
Hello, there is no newer version available, the latest FW is V2.0. Regards |
Follow us on