5/26/2014 11:31 AM | |
Posts: 88 Rating: (12) |
Hello abdel-qader, I have a beginning of answer for you: 1. No, see the link below: http://support.automation.siemens.com/WW/view/en/88779346 2. Yes 3. Yes 4. Yes 5. Apparently, the firmware is valid for all S7-1200 CPU but be carefull because order number is different: for example they have 6ES7214-1AG31-0XB0 for V3.0 and 6ES7214-1AG40-0XB0 for V4.0. So I don't think it's possible to "upgrade the firmware" Perhaps somebody else can confirm that. 6. I don't know if it is related to WinCC but obviously it is recommended 7. Yes it's as of firmware version 2.0 see the link below: http://support.automation.siemens.com/WW/view/en/86217872 Best regards, |
Last edited by: Kelu at: 5/26/2014 11:57 AMLast edited by: Kelu at: 5/26/2014 11:55 AMLast edited by: Kelu at: 5/26/2014 11:36 AM |
|
This contribution was helpful to1 thankful Users |