8/1/2020 2:54 PM | |
Joined: 9/27/2006 Last visit: 5/4/2024 Posts: 12257 Rating: (2666) |
Hello kouim_kostas; Not knowing which version of TIA Portal was used to program your PLC can be problematic. Does the message not provide any information on the version of Step 7 used? Can you provide a screenshot of the error message? Here is a FAQ discussing this issue, with possible workarounds, and a discussion of the contents of that FAQ: What options are available in STEP 7 (TIA Portal) for uploading when the project version in the CPU no longer matches the version on your PG/PC? https://support.industry.siemens.com/cs/ww/en/view/97554052 Tia Portal Upload Problem Could you also give us the model number and hardware version of the S7-1200 you are using, it could have an impact on your ability to use TIA Portal v15.1 to program it. Hope this helps, Daniel Chartier |
8/1/2020 3:21 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, Have a look at the attached file. What is the version of TIA Project? This is supported by some types of CPU . |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to2 thankful Users |
8/2/2020 1:50 PM | |
Joined: 5/3/2018 Last visit: 5/1/2023 Posts: 22 Rating: (0) |
i attached a zip file with the errors i mentioned before.!
Attachmentzip.zip (122 Downloads) |
8/2/2020 3:42 PM | |
Joined: 3/28/2015 Last visit: 4/19/2024 Posts: 721 Rating: (213) |
Hello, CPU: 6ES7215-1AG40-0XB0 V 4.0 I suggest to install TIA V13 SP2 Software and use it to perform the upload of the PLC program. TIA V15 Software licence is valid for the earliest TIA versions. Perhaps the following topic might help: TIA V13 SP2 |
Eng.Mohamed Ibrahim |
|
This contribution was helpful to1 thankful Users |
8/3/2020 3:29 PM | |
Joined: 5/3/2018 Last visit: 5/1/2023 Posts: 22 Rating: (0) |
Hello... I install TIA V13 SP2 Software and it worked fine.! I manage to upload the PLC program.! Thank you very much for your help. [snip] |
Last edited by: Jen_Moderator at: 08/04/2020 08:18:29Division of questions into separate topics. |
|
This contribution was helpful to2 thankful Users |
Follow us on