6/18/2018 8:33 PM | |
Joined: 2/20/2016 Last visit: 11/4/2020 Posts: 4 Rating: (0) |
Dear All, I'm currently working on TP V13 SP1, and finally I've faced a problem - here is the CPU1211 FW4.2 which is supported only with TP >= V14 (as per catalogue). So I thnk I have to install TP V15. I have a number of projects done in V13 SP1. So could you please advice 1. Can TP V15 be installed and run in parallel to V13 SP1? 2. Can TP V15 successfully convert projects from V13 SP1? (i've heard before at this forum(?) that there were problems in V14 with converting projects from V13) Thank you! ------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 6/19/2018 8:16:07 AMNew subject after splitting |
|
3/20/2019 4:16 PM | |
Posts: 3 Rating: (0) |
Great answer #dP ¿Is there an official text from Siemens saying that? Thanks, Pablo |
Follow us on