(0)| 10/27/2015 12:43 PM | |
|
Posts: 24 Rating:
|
Dear Michael K, my method to change the netcard is shutdown the virtual machine, close down VMware and manually edit .vmx file on Notepad, setting for example: ethernet0.virtualDev = "e1000" or ethernet0.virtualDev = "vmxnet3" Then, when I run the virtual machine, the driver is automatically installed. See the attached .vmx file (as .txt) Best Regards, fredito AttachmentVM - TIA Portal 13 SP1 - copy.txt (628 Downloads) |
Last edited by: fredito at: 10/27/2015 12:49:41 PM |
|
| 10/28/2015 6:23 AM | |
|
Joined: 5/12/2006 Last visit: 10/24/2025 Posts: 22738 Rating:
|
this is wrong! TIA V13 support and is released for Win7 32bit Operating System. You can check this with the compatibility tool! Regards Christoph AttachmentSTEP-7-Professional-(TIA-Portal)_V13.0_compatibility-list_en_2015-10-20.xlsx (450 Downloads) |
| 10/28/2015 1:55 PM | |
|
Posts: 24 Rating:
|
Yes, ChristophD, you are right, in fact:
Anyway, I'm now installing TIA Portal V13 SP1 on Windows 7 64-bits (Virtual Machine) Best Regards, fredito |
| 1/15/2016 9:00 AM | |
|
Posts: 15 Rating:
|
I would like to try NIC Vlance on win7 machine? It works for XP... But, I can't find drivers for AMD 79C970 PCnet32 LANCE for win7. Does it even exist? |
Follow us on