8/13/2013 5:54 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Hello Sandman Can we use TIA Portal with SIMOTION SCOUT ?? As of Scout V4.3, I think it only supports WinCC Flexible. Also as correctly pointed out by Techteam the Lowest HMI supported by SIMOTION is TP177B Cheers Navnag |
Last edited by: Navnag at: 8/16/2013 3:25 PMLast edited by: CS Moderator at: 8/16/2013 2:01 PMnew subject after splitting from /tf/WW/en/Posts/96082#top There is no such thing as the last bug in a program |
|
8/21/2013 2:01 PM | |
Posts: 3037 Rating: (192)
|
Hello, You can see which software works togehter with WinCC TIA Portal in this link. http://support.automation.siemens.com/WW/view/en/51694087 Tweety |
9/1/2013 10:02 AM | |
Joined: 11/21/2007 Last visit: 3/14/2024 Posts: 2323 Rating: (307) |
Thanks Tweety I think, I did not phrase my question properly ... What I meant was, Can SIMOTION SCOUT ( or SINAMICS STARTER ) be integrated into TIA portal as in STEP7 V5.x ? i.e. all the Drive / SIMOTION settings and data are stored within the STEP7 project. If not, then what is the alternative available ? Thanks Navnag |
There is no such thing as the last bug in a program |
|