6/23/2016 10:53 AM | |
Posts: 5 Rating: (0) |
Hello Christoph, It's good to hear that the connexion is well done. What do you means by "download all data" ? I "downloaded to device", through TIA and also through TIA-SCOUT with success. No compilation error. But in this case, why there is some red notification in the project tree ? The CX32-2 appears "not reachable, Error in lower level components" I'm not sure that I will success to use the digital I/O of the CX32-2 In fact, I can't RUN the D425-2 device. The D425-2 remains on STOP. Leds on the devices are like a chrismas tree ! To help to understand I created this dropbox link with more files https://www.dropbox.com/sh/k2zkef34ei8ny6e/AACir79O_kUuGEpB3dMXX95za?dl=0 edit: I just saw that when I go online within SCOUT I have some error message with CX32-2 devices. Then I can acknowledge these messages and run the servomotors. (See picture attached) Many thanks. |
Last edited by: Indutech at: 6/23/2016 10:55:26 AMLast edited by: Indutech at: 6/23/2016 11:04:11 AMLast edited by: Indutech at: 6/23/2016 11:16:26 AM |
|