2/14/2016 7:27 PM | |
Posts: 3 Rating: (0) |
Dear experts , Right now am using KTP 700 basic panel with tia porta v13 & plc is s7-1200 .In hmi i had created the momentry buttons for start ,stop ,reset, accept .with memory bits from m10.0 ---m10.5 . all these buttons are momentry . While i giving the start momentry but i made an configuration like in events i had given for press i had given set bit & tagged the address & in release i had given the reset bit & tagged the addrees
But the problem is when i press the button it is is set but not reseted so the button becomes switch type & gets latched with the output even though i tried with other options like set while key pressed in events also but the momentry type is not working kindly p[lease any one give the solution for this ------------------------------------------------------------------------------------------ |
Last edited by: Min_Moderator at: 2/15/2016 11:43:24 AMNew subject after splitting |
|
Follow us on