5/31/2018 2:35 PM | |
Joined: 2/12/2016 Last visit: 2/1/2021 Posts: 16 Rating: (2) |
Dear all two days ago during comissioning visit at the customer my TIA portal installation started crashing when I tried to open any project, or to create a new one. Today I noticed that it even crashes if I just click Online Access without any project activated. I know that the version is old, and one solution is to re-install, I already tried to do "Repair" installation and re-installed Update 9 for SP1 but again no help. I have already downloaded V13 SP2 and this is the next step to do tomorrow if there are no new ideas what could cause this. Crash report as attachment. Attachmente5af5882-83d8-4293-8e7f-4918c083173e.zip (57 Downloads) |
Follow us on