2/18/2019 2:06 PM | |
Joined: 4/24/2006 Last visit: 9/24/2024 Posts: 8742 Rating: (1168)
|
Hello Vishakha, Perhaps this link might help: USB Recovery (Reset to factory) Mode for 2nd Generation Basic Panels Best regards, Wizard |
2/18/2019 2:15 PM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
It is said in document that "Start recovery" button will come but after I connect nothing comes and HMI screen remains as it is. Any suggestion ?? Do I have to go into some settings on HMI for doing the recovery???or it will ask automatically after connecting the pen drive and power recycle???
|
2/19/2019 1:23 PM | |
Posts: 64 Rating: (7) |
Hi Vishakha, Here is a link to a Siemens FAQ on the subject, it says the following:
I hope this can help you towards a solution |
3/26/2019 2:16 PM | |
Joined: 9/21/2012 Last visit: 9/25/2024 Posts: 4165 Rating: (464) |
Are the files on the USB stick, as Siemens states they need to be? |
3/27/2019 12:31 PM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
Yes the image file as per mentioned in the manual is only copied to the usb. |
3/27/2019 1:33 PM | |
Joined: 9/21/2012 Last visit: 9/25/2024 Posts: 4165 Rating: (464) |
Did you extract the ZIP? to the root of USB drive? |
Follow us on