2/18/2019 1:06 PM | |
Joined: 2/8/2018 Last visit: 3/28/2023 Posts: 256 Rating: (4) |
I too have the same problem but my HMI is KTP400 basic . I am not able to solve the problem as the image file installed on HMI is version 15 and i have version 14.01 So when i try to download , it asks for same Overwrite and Fit , but after selecting it..it doesnt download and gives the error of " Adaptation of target device failed" Now when m trying to do os update and reset to factory settings , nothing is happening no error message and no info. Please help.
------------------------------------------------------------------------------------------ |
Last edited by: Jen_Moderator at: 2/27/2019 2:04:57 PMNew subject after splitting |
|
2/27/2019 2:06 PM | |
Joined: 6/19/2017 Last visit: 9/6/2024 Posts: 8175 Rating: (172) |
Closed cause question posted twice. The second thread with the subject TIA V14 SP1 download error on KTP400 Basic is published within the conference SIMATIC Panel. Best regards Jen_Moderator |
Follow us on