10/13/2018 11:25 PM | |
Posts: 14 Rating: (0) |
Hello, I want to upgrade my TIA v14. I installed sp1 or sp4. I get this warning at the photo. What is the problem? |
10/14/2018 4:20 AM | |
Joined: 10/7/2009 Last visit: 8/19/2023 Posts: 266 Rating: (92) |
Dear Engin Safak, The message says that you need an existing V14 SP1 installed on your PC, but you don’t' have. You can download the TIA V14 SP1 from this link: SIMATIC STEP 7 including PLCSIM V14 SP1 TRIAL download which can be used to upgrade existing V14 installations as well as for new installations. Once installed TIA V14 SP1, you can then install the UPDx using Automation Software Updater. Best regards, Yu-wen |
Last edited by: Yu-wen Tang at: 10/14/2018 4:22:21 AM |
|
10/17/2018 10:25 PM | |
Posts: 14 Rating: (0) |
Thanks for reply. |
5/18/2021 10:37 AM | |
Joined: 4/16/2020 Last visit: 12/14/2021 Posts: 5 Rating: (0) |
Thank you for your answer, unfortunately I did not find on the siemens site the sp1 without the updates |
Follow us on