9/24/2021 11:56 AM | |
Joined: 4/8/2021 Last visit: 4/25/2024 Posts: 25 Rating: (0) |
Good day, I am running into an issue when it comes to deactivating runtime. Every time I deactivate the runtime, it gets stuck at 28%. I've never troubleshot WinCC before, so I apologize for not understanding diagnostic logs. I'm running WinCC RT Professional Version V14.0 SP1 UPD10 (running on windows 10). I have another project that works perfectly fine. I compared all of the settings and configurations from the TIA projects and everything matches (as far as I can tell). The same project is also running on WinCC RT Professional Version V14.0 SP1 UPD6 on a different PC without issues. Recompiling the project didn't work. I have absolutely no idea how to begin to narrow down the issue. Please see screenshot below. Global Script? Where do I view this script? Is this SCADA related? Is the issue somewhere in the HMI scripts? Please help. [snip] AttachmentPMD_Log.txt (69 Downloads) |
Last edited by: Ruskied at: 09/24/2021 12:08:18Last edited by: Jen_Moderator at: 09/24/2021 12:59:16Added log as txt. file. |
|
Follow us on