1/13/2012 2:24 PM | |
Posts: 3037 Rating: (192)
|
Hello,
You have two different Runtime, one for advanced (TP 1200), one for Professional. The faceplate of Runtime advanced does not work in Runtime Professional. Here is an example of faceplates of WinCC Classic. Example blocks for STEP 7 and WinCC Then you migrate form WinCC V7 to WinCC V11 SP2 Tweety |
1/16/2012 11:59 AM | |
Posts: 3037 Rating: (192)
|
Hello, This is onlyfor WinCC Classic: Here is an example of faceplates of WinCC Classic. Example blocks for STEP 7 and WinCC This is for WinCC V11 Professional: You must create the faceplate for WinCC Runtime Professional new. You can not use a faceplate of WinCC Runtime advanced (TP1200) or a Faceplate of WinCC Classic. You can findmore information of faceplatein thefollowing link. see the chapter 9.1.7. WinCC Professional V11.0 SP2 Tweety |
1/17/2012 2:48 PM | |
Posts: 3037 Rating: (192)
|
Hello, you can contact the customer support for your behaviour. ----> customer support Tweety |
Last edited by: Tweety at: 1/17/2012 2:48 PM |
|
1/17/2012 3:59 PM | |
Posts: 26 Rating: (0) |
Thank you. I have done so, and submitted a support ticket. Both parties are unable to do this.
|
1/26/2012 11:42 AM | |
Joined: 4/29/2010 Last visit: 3/19/2024 Posts: 1557 Rating: (161)
|
In this case yes, because of the animation -> visibility. |
1/26/2012 6:04 PM | |
Posts: 26 Rating: (0) |
Ok so I have figured it out with the help of South African support. Support in Germany also said...impossible for visibility. I still think it is something the developers overlooked, because you have to script it in VB (normally means it is not supposed to be like that) I am still dissapointed in the software - there is a SH*Tload of developing work to be done by Siemens to finish this off. Launch was done far before the software was ready IMHO. Siemens is using the man on the street to fix their software, but then again so is Microsoft. Sample attached Attachment2012-01-26.FaceplateBitStripping.zip (337 Downloads) |
This contribution was helpful to1 thankful Users |
6/27/2014 6:35 PM | |
Joined: 3/25/2013 Last visit: 3/21/2019 Posts: 176 Rating: (1) |
New question split intoslow response from the HMI when using multiple faceplates in one screen. With best regards, Narrator1
|
Follow us on