1/26/2012 11:42 AM | |
Joined: 4/29/2010 Last visit: 1/20/2025 Posts: 1557 Rating:
|
In this case yes, because of the animation -> visibility. |
1/26/2012 6:04 PM | |
Posts: 26 Rating:
|
Ok so I have figured it out with the help of South African support. Support in Germany also said...impossible for visibility. I still think it is something the developers overlooked, because you have to script it in VB (normally means it is not supposed to be like that) I am still dissapointed in the software - there is a SH*Tload of developing work to be done by Siemens to finish this off. Launch was done far before the software was ready IMHO. Siemens is using the man on the street to fix their software, but then again so is Microsoft. Sample attached Attachment2012-01-26.FaceplateBitStripping.zip (473 Downloads) |
This contribution was helpful to
1 thankful Users |
6/27/2014 6:35 PM | |
Posts: 176 Rating:
|
New question split intoslow response from the HMI when using multiple faceplates in one screen. With best regards, Narrator1
|
Follow us on