8/7/2014 8:31 AM | |
Posts: 12 Rating: (0) |
Unfortunately, i couldnt find a solution. I still cant connect. |
8/7/2014 8:45 AM | |
Posts: 12 Rating: (0) |
Ip configuration => Ok Simatic IEPG Help Services => Started Set PG/PC Interface =>I Chosed TCP/IP(Auto) But i still cant go online.
|
11/27/2014 5:28 PM | |
Joined: 9/3/2012 Last visit: 2/6/2024 Posts: 5 Rating: (0) |
Hi. I have the same problem, running win7 64bit +Step7+WinCCFlex+TIAv13+... Everything was working good for some months until I needed a MicroWin software. After installing MicroWin this error appeared ("Cannot load the selected communication driver:file not found"). So after removing MicroWin and some reinstalls ot TIA and Step7 the result is the same. Before with Win XP I also used the trick with "SIMATIC IEPG Help Service", but now in Win7 64bit there is no such a service . I tried to start or restart all other "SIMATIC" and not only SIMATIC services but also with no result. So after some days of tries I'm starting from a new Windows installation. Any ideas about how this error can be fixed or what is the new name of the service? Or any other way that the communication driver can be repaired? This error is only for Ethernet communication. MPI and Profibus works normally. |
12/20/2014 1:06 PM | |
Posts: 1 Rating: (0) |
Hi, I've the same issue. Neither reinstallation of Step7 nor uninstall of MicroWin helped. Anybody has found a solution ?
|
1/28/2015 9:19 AM | |
Posts: 5 Rating: (0) |
hey, i have the same problem and i did not found the solution... ( |
3/23/2015 3:02 PM | |
Joined: 5/20/2014 Last visit: 7/19/2023 Posts: 6 Rating: (0) |
same problem.. missing "S7ONLINX64.dll" no work if reinstall all.. i think only solution its format PC :( .. |
3/25/2015 10:35 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4774 Rating: (123) |
|
Follow us on