Industry Online Support
Technical Forum
2/14/2012 11:39 PM | |
Joined: 1/28/2009 Last visit: 5/2/2024 Posts: 6838 Rating: (1359)
|
Dear Nikzitronik, To get a better result, you have option of revising your calculations and consider your base time values around 100ms. If so you can use S5 timers,IEC timers or even OB3X with negligible error.Pulses period can be adjusted dynamically by comparing value used to reset C0. [code] AN M 100.0 = M 100.0 //////////////////////////////// A M 100.0 CU C 0 NOP 0 L C 0 L 1 ==I JCN hd1 SET = M 100.1 JU out hd1: CLR = M 100.1 out: NOP 0 L C 0 L 19 //dynamize ==I R C 0 [/code] Best regards, Hamid Hosseini |