2/21/2007 4:11 PM | |
Joined: 12/5/2005 Last visit: 4/16/2024 Posts: 239 Rating: (9)
|
Hi Sandromig, Why you don't use the messages exported from PAS of your IED? I didn't understand the reason. Well, I already made this, but I used WinCC (wasn't SICAM WinCC for SAS and wasn't SICAM PAS CC) and SICAM PlusTools with the PLC. |
Márcio Santos |
|
2/21/2007 9:09 PM | |
Joined: 12/5/2005 Last visit: 4/16/2024 Posts: 239 Rating: (9)
|
Hi Sandromig, So, as I don't know deeply the SICAM PAS, maybe I can't help in the best way. I only find strange you it can't create messages for double points in the 4 states (00,01,10 and 11). As I had mentioned in the previous post, In my company we created functions in the PLC for read, store and send the messages to WinCC. In this case the PLC send the Number, Status and the TimeStamp of Message. In the WinCC, scripts using MSRTStartMsgService, MSRTCreateMsg and MSRTStopMsgService functions, save the message in the DB of WinCC. In this way, it is easy to configure messages in the WinCC, the only tasks be, set the message number, your Class and Type. The hard task be running in the PLC. Perhaps, you can request a support direct from PTD. Go to http://www.sicam.de/index_e.htm. |
Márcio Santos |
|
Follow us on