6/7/2012 6:42 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello worldleader, The reason is somehow explained here:
To test the idea, I make an FC and call it in OB1. I download the program into the PLC and no problem would be appear while uploading and opening the blocks. (pic#1 in the attachment). Now, I change interface of FC1 by simply adding another input to the function, save it and download it without updating where it is called in OB1.Then I download FC1 to PLC. (pic#2 in the attachment). Now, I upload the program from PLC and see what happened.This is the case you are looking for.(pic#3 in the attachment). To avoid this case, simply when changing a block parameter, update it in all 'caller" blocks.More information in Chapter 15 of this manual. (Especially section 15.2) http://support.automation.siemens.com/WW/view/en/45531107 Best regards, Hamid Hosseini Attachmentts.conflict.zip (971 Downloads) |
This contribution was helpful to7 thankful Users |
6/8/2012 2:44 AM | |
Posts: 22 Rating: (1) |
Thank you, hdhosseini! I can understand why this is happened. I really appreciate it again! |
This contribution was helpful to1 thankful Users |
8/6/2013 9:23 AM | |
Posts: 45 Rating: (1) |
Dear worldleader, i am getting same error please tell me how to update "caller" block. your mentioned link is not opening. Thanks and regards, Doggalli |
8/6/2013 9:54 AM | |
Joined: 1/21/2013 Last visit: 3/19/2024 Posts: 4618 Rating: (705) |
Hi doggalli, follow our friend Hamid Hosseini it's easy. |
This contribution was helpful to1 thankful Users |
9/14/2023 11:54 AM | |
Joined: 2/13/2023 Last visit: 2/2/2024 Posts: 1 Rating: (0) |
I'm facing the same issue with time stamp conflict error. |
11/10/2023 6:44 AM | |
Joined: 6/28/2020 Last visit: 4/13/2024 Posts: 2 Rating: (0) |
Hi bro. Modify proplem, can you show me? thanks |