11/13/2008 2:46 PM | |
Posts: 103 Rating: (10) |
Please clarify your question. Do you want to use a time of day for when an input is triggered or for when the hardware config was changed or something else? |
11/13/2008 2:59 PM | |
Posts: 162 Rating: (23) |
Hi SM, maybe this helps link here? http://support.automation.siemens.com/WW/view/en/15218045 Best regards FrankW |
11/15/2008 11:48 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
So I understand that without ET200M,I couldn't use time stamp in input module.Am I right? |
11/16/2008 12:32 AM | |
Joined: 7/2/2008 Last visit: 4/5/2024 Posts: 928 Rating: (305) |
Yes, you have to use ET200M but the point is (IS IT POSSIBLE TO DO IT WITH S7-300?). According to this FAQ, it is only possible with S7-400 but if you take a look at ET200M manual which you can find in Dchartier's replyto this thread, you will find that you can use precise time stamping feature outside S7-400 with a CPU with integrated DP clock master but it's not stated clearly that it can be S7-300 CPU (Page 127/290). I hope one of the forum's experts would tell us if it is possible or not. |
11/26/2008 11:45 AM | |
Joined: 11/8/2005 Last visit: 2/15/2024 Posts: 335 Rating: (3) |
Is there any example which is implemented "time stamping" on it (especially in S7-300)? |
1/7/2009 3:56 PM | |
Joined: 8/10/2005 Last visit: 4/9/2024 Posts: 1486 Rating: (32) |
within the thread Time forwarding in S7-300 Aret published the following information:
|
Follow us on