7/30/2020 4:41 PM | |
Posts: 34 Rating: (3) |
Hi, I am running WinCC application on V7.4 with 1 server and 3 clients. I configured the time synchronisation and the server parameters and the client parameters as per the screenshots. ( The server takes the time from the Wincc Server and the clients take the time from the Server) Now when i change the time on the server by adjusting time settings, the application running on the server only gets its time updated ( expected ) however the clients did not ( why?) The clients only get their time updated when i change the time from the date and time settings of each client. Can you please help me figure out why? Thanks AttachmentScreenshots.docx (42 Downloads) |
8/5/2020 5:00 PM | |
Posts: 34 Rating: (3) |
Hi george, yes the clients are configured to run it on startup thanks |
Follow us on