6/1/2007 4:24 AM | |
Posts: 122 Rating: (4) |
dear experts: my WINCC project is a single-user-project.and it didn't use "time synchronization" before(see my document"old synchronization settings") one day i tried to activate the "synchronization via system bus(master,slave)/access point 1",it was no problem, but when i change back to the original settings,it said that this operation is forbidden(see document"time synchronization"),so i can not deactivate the synchronization anymore,i don't know why. how can i cannel the "time synchronization"? Attachmentsynchronization.zip (94 Downloads) |
6/1/2007 9:06 AM | |
Posts: 3149 Rating: (171)
|
Hallo are you using WinCC or WinCC Asia? Which Microsoft operating system is installed? nemo |
6/1/2007 9:58 AM | |
Posts: 122 Rating: (4) |
WINCC, windows 2000 professional. |
6/1/2007 11:03 AM | |
Posts: 3149 Rating: (171)
|
Hi |
6/4/2007 1:58 PM | |
Posts: 1275 Rating: (123)
|
Hi, Your diagnose folders should be under "...\Siemens\WinCC\Diagnose", by default "C:\Program Files\Siemens\WinCC\Diagnose"... Best regards, Danielle |
6/6/2007 8:47 AM | |
Posts: 122 Rating: (4) |
dear experts: i have already solved the deactivating problem and it can not be successful before just because that my methods of deactivating was wrong,and i also correted the time offet after deactivating the time synchronization.(see document "wrong deactivating"/"right deactivating") thanks very much! Attachmentdeactivating.zip (92 Downloads) |
6/6/2007 1:36 PM | |
Posts: 1275 Rating: (123)
|
Glad it's working. Thanks for posting your solution. Best regards, Danielle |
7/22/2013 11:43 AM | |
Joined: 4/24/2009 Last visit: 2/19/2024 Posts: 2683 Rating: (135) |
Follow-up-question splitted to when am opening runtime after few seconds my Server time advancing to three hours Best regards O_Moderator |
Follow us on