6/15/2015 2:45 PM | |
Posts: 45 Rating: (0) |
Dear, can anyone guide me how many timers counters and memory bits we can call in the simatic s7 300 series cpu 317 2pn/dp? regards |
6/15/2015 2:59 PM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello, Range of maximum number simatic counters ,timers plus max number of flags , you need to check the specification of a CPU.To access that, you need to search the exact order number of CPU.As an example check:
6ES7317-2EJ10-0AB0you need to check entries for:
I hope this helps, hdhosseini |
Last edited by: hdhosseini at: 6/15/2015 3:03:03 PM |
|
This contribution was helpful to3 thankful Users |
11/22/2015 8:36 AM | |
Posts: 45 Rating: (0) |
Assalamualaikum i have gone through the picture but i just have a doubt what is 512 is it numbers or is it size in logic if it is numbers then do tell me one thing if my logic or my operation need more than that then how can i enhance or can it be enhance by adding external memory card Regards |
Follow us on