10/29/2020 5:30 PM | |
Joined: 9/23/2005 Last visit: 4/17/2024 Posts: 4325 Rating: (1419)
|
Hi, The Application Example "Connecting a SIMATIC HMI operator device with a SIMATIC S7-1500R/H" (https://support.industry.siemens.com/cs/br/pt/view/109781687/en) shows two ways to connect an HMI to a S7-1500R/H:
The related project, however, doesn't shows how this second option could be done in WinCC Unified. So, some tips for this implementaion:
Attached there is a sample project. I used two S7-1500 non redundant to enable simulation in PLCSim Advanced. AttachmentUnifiedRedundantConnection_20201030_0644.zip (794 Downloads) |
Last edited by: Denilson Pegaia at: 10/30/2020 10:47:35redundancy control optimized Last edited by: Denilson Pegaia at: 10/30/2020 10:49:10link revised Denilson Pegaia |
|
This contribution was helpful to2 thankful Users |
11/20/2020 11:09 AM | |
Posts: 22 Rating: (0) |
Hi Thanks for the example above, is there any example in TIA V15.1. We just got 15.1 through our cooperate IT and siemens have moved on to v16. Would appreciate if you can convert 16 into 15.1 and share it.
|