Industry Online Support
Technical Forum
1/27/2015 2:59 PM | |
Joined: 9/23/2005 Last visit: 4/29/2024 Posts: 4325 Rating: (1425)
|
Hi, A new feature that STEP7 V13 SP1 brings is the new instructions, "GetInstancePath" and "GetSymbolPath", for the creation of customer-specific message texts are also available. An overview of the new instructions is provided in the list of comparison (entry ID 86630375) Requirements: CPU S7-1500 FW >= 1.7 (http://support.automation.siemens.com/WW/view/en/106192301 ) STEP 7 >= V13 SP1 One possibility of useis to showin WinCC pictures / alarmsan identification offield objects, with low engineering work. In the follow sample program they are used together with GetBlockName, GetInstanceName and GetSimbleName to be monitored in Watch Table to add text to alarms (not all variables, I know that there is others ways to do it). Together with the program there are also some print screens. Attachmentexample.zip (225 Downloads) |
Last edited by: Min_Moderator at: 1/27/2015 4:23 PMReupload attachment Denilson Pegaia |
|
Follow us on