6/24/2013 12:14 PM | |
Posts: 8 Rating: (0) |
Hello, Can someone tell me if TM1703 eMic can be programmed as an IEC104 master?
|
6/24/2013 12:53 PM | |
Posts: 12 Rating: (1) |
What for it you? 1703eMic has only one serial or LAN/WAN interfaces. how it will send data?
|
Last edited by: anfimichev at: 6/24/2013 1:27 PM |
|
6/25/2013 7:02 AM | |
Posts: 12 Rating: (1) |
I think no. We use "TMeMic" for other goal. |
6/29/2013 11:00 PM | |
Joined: 11/18/2009 Last visit: 8/17/2023 Posts: 262 Rating: (18) |
If you have more then 500 signals emic is not good for you. Best Regards Ensar |
7/1/2013 7:22 AM | |
Posts: 8 Rating: (0) |
Thank you all for replying. The emic i am talking about doesn't need to handle more then 100 signals. |
Last edited by: claud84 at: 7/1/2013 7:23 AM |
|
7/1/2013 8:37 AM | |
Joined: 11/18/2009 Last visit: 8/17/2023 Posts: 262 Rating: (18) |
Emic can't be master and slave. emic has only 3 interfaces. One is ethernet. For this you can use TM. |
11/5/2013 1:19 PM | |
Posts: 36 Rating: (2) |
no it is not possible, you can go for higher rtu which tm1703. this can support more protocols and has more interface forserial/lan. |
12/23/2013 8:19 AM | |
Posts: 9 Rating: (2) |
Emic support device function in controlled station (Slave) mode only. see more detail as per attached. Item 7.1 System or device function (p.3) AttachmentD:\can delete\Pages from IEC_60870_5_101_104_ACP_ENG.pdf (148 Downloads) |
This contribution was helpful to1 thankful Users |
Follow us on