Industry Online Support
Technical Forum
6/6/2013 11:44 AM | |
Joined: 2/1/2011 Last visit: 9/13/2023 Posts: 186 Rating: (4) |
Dear Sir, Actually I wanted to display event in Wincc For the Master change over and Present master of S7 400 H PLC system. Meanwhile going through Forums, Found one forum which provide the redundant tool: Redundant Tool In this when calling FB6 there are two inputs to be provided. As I am new to H system please tell me what value to put for master system number(FB6 Input) for CPU 0 and CPU 1. In hardware configuration where I can found. |
6/7/2013 7:06 AM | |
Joined: 1/28/2009 Last visit: 4/1/2024 Posts: 6836 Rating: (1359)
|
Hello, As mentioned in comments of the program, you find the "Master System Number" in HW.Config as shown in the attachment.That is also for node diagnosis on PROFIBUS as SFC51 is called with SSL-ID "W#16#292" Best regards Hamid Hosseini |
Follow us on