10/22/2018 1:24 PM | |
Joined: 10/11/2006 Last visit: 5/14/2024 Posts: 5838 Rating: (790)
|
Hello, this is really up to you. There is almost no difference. The only difference is using telegram 1 and SINA_SPEED FB or using technology object and programming with PLC open commands (MC_Power,...). Anyway you can use the PROFIsafe telegram additionally to your standard telegram. By the way: There are ready-to-use safety function blocks to communicate with the safety telegrams: https://support.industry.siemens.com/cs/ww/en/view/109485794 |
With best regards, |
|
This contribution was helpful to1 thankful Users |
10/22/2018 3:24 PM | |
Joined: 10/11/2006 Last visit: 5/14/2024 Posts: 5838 Rating: (790)
|
Hi, if you want to save performance on the PLC side and want to add additional data to the telegram I would recommend to use the SINA_SPEED block (so no technology object) and add supplementary data to the telegram. This can be read out by system function GETIO(_PART). Please see this post if you are interested on how to program the cyclic communication: https://support.industry.siemens.com/tf/ww/en/posts/telegrams-adaptive/201376/?page=0&pageSize=10 |
With best regards, |
|
10/22/2018 3:38 PM | |
Joined: 9/21/2012 Last visit: 5/13/2024 Posts: 3937 Rating: (444) |
Or you can use the internal PID of the G120. |
10/22/2018 4:07 PM | |
Posts: 15 Rating: (0) |
Thank you,, but where can I find this telegram library? |
10/22/2018 4:40 PM | |
Joined: 10/11/2006 Last visit: 5/14/2024 Posts: 5838 Rating: (790)
|
Hi, ok, now I know. There are system UDTs available for all telegrams that can be used with any technology object (e.g. Tel 3, 5, 105,...). You will not see them by autocompletion. You need to type them as: PD_TEL3 or PD_TEL105 for example, then you get the telegram structure. There is also an additional telegram library available in SIOS for some telegrams that are not implemented as system UDTs: https://support.industry.siemens.com/cs/ww/en/view/82841762 (in this case you need to copy the UDT from the library to the PLC datatypes and then you can create a variable of this type) But you can also type the structure manually. This is also possible if you do not find the suitable UDT for your application. |
With best regards, |
|
This contribution was helpful to1 thankful Users |
10/22/2018 4:47 PM | |
Posts: 15 Rating: (0) |
Thank you very much :) |
Follow us on