2/4/2009 8:31 AM | |
Posts: 272 Rating: (4) |
Dear All, |
2/4/2009 8:54 PM | |
Posts: 2661 Rating: (279)
|
Hi Prateek, Yes, this is possible as Jaapie has stated. Right-click on the object (for example MOTOR) and click on Configuration Dialog and then drag and drop the Tooltip Text property on to the Selected Properties. See FIG 1 in attachment. However, there are someimportant points worth noting especially if you want to use the "Generate/Update Block Icons" feature:
Regards AttachmentStandardBlockIcons.pdf (297 Downloads) |
Last edited by: Phantom75 at: 2/4/2009 8:58 PM |
|
2/5/2009 9:41 AM | |
Posts: 272 Rating: (4) |
Hi Jaapie, Can i change the TTT aumatically for all the block icons in the project? |
2/5/2009 11:45 AM | |
Posts: 272 Rating: (4) |
Jaap, How to do that?? |
2/6/2009 7:33 AM | |
Joined: 1/17/2006 Last visit: 4/16/2024 Posts: 800 Rating: (63) |
OOPS, this "several attributes behind a property solution" does not work with a TTT. There is an error....strange (anyone knows why?). So I made you an example to do it. It is nice too. I hope this helps. I made an extra property Tool Tip Text and fill it with a script when the tagname changes. You also can type the tool tip text in within graphics designer then you do not need the script. Changing tagnames of objects is not nice I think. Good luck AttachmentTTT.zip (210 Downloads) |
Follow us on