9/5/2019 1:54 PM | |
Joined: 3/12/2015 Last visit: 11/29/2023 Posts: 529 Rating: (15) |
My library... |
9/6/2019 6:37 AM | |
Joined: 4/23/2010 Last visit: 12/31/2023 Posts: 8092 Rating: (872)
|
Hello, How long this machine was down i.e. power was switched OFF? What alarm/error/fault is displayed? Please attach snap shot. Do you have NC PLC data back up? Which drives are installed? Sinumeric or Sinamics? Attached Library screen shot where from taken? Not clear. You need to set TCP/IP network properties & set IP address. For X127 port IP address is 192.168.215.1 NCU MLFB number is provided on sticker which is at right side cover of NCU. Please refer attached snap shot. From NCU MLFB PLC CPU details can be confirmed. 6fc5203-0af00-0aa1 is OP & not HMI software. HTH |
7/9/2021 9:03 PM | |
Joined: 2/27/2021 Last visit: 4/24/2024 Posts: 1 Rating: (0) |
Hi did you got this solved? Im having the same error |
8/8/2021 7:09 PM | |
Joined: 7/29/2021 Last visit: 1/26/2024 Posts: 1 Rating: (0) |
Conseguiu comunicar com sinumerik 840d? |
Last edited by: higomelo at: 08/08/2021 19:13:14 |
|
Follow us on