4/21/2008 4:05 PM | |
Posts: 39 Rating: (9) |
Hello Andrew, when the torque limiting is active with the command _enabletorquelimiting, the drive is build-up maximal with the programmed limit. That means the maximal actual torque must be equal to the programmed limit. When torque limiting is active it is possible to make axis positioning. Normally the axis must not stop during active torque limitation by an error. Maybe the command _enabletorquelimiting is not active. Which error comes up? I attached a screen shot with a list of important parameters and the FAQ. Best regards ThomasD Attachmenttest.zip (799 Downloads) |
Follow us on