5/22/2012 7:08 PM | |
Joined: 10/7/2005 Last visit: 5/13/2024 Posts: 3005 Rating: (1048)
|
Trust me it can dear m.shoaib khatana, because you end upadding a tiny bit too small value thousands of times to an ever increasing total. It's yourcall at the end of the day what you want to test or try though. If you want to be really precise,I forget to mention the best way to do totalising which is: Use a Digital Output of your Flowmeter (it should have one, most do anyhow), connect it to a free DI, configure the Flowmeter to give you a pulse perx amount and then simply add up the pulses (doing Totalsbased on AI will never be 100% accurate even if Siemens provides you with a block for this purpose). The only thing to look out for is to make sure that the DI pulses are not missed (i.e. they are long enough andand don't come faster that the scan of the logic that evaluates them). I hope this helps |
Cheers |
|
This contribution was helpful to2 thankful Users |
2/15/2016 11:52 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4773 Rating: (123) |
New question published by AutoGen_905449 is split to a separate thread with the subject Block FB100 "Totalizer" for step7 5.5 and LAD programing. Best regards |
2/19/2016 10:10 AM | |
Joined: 9/3/2014 Last visit: 3/13/2019 Posts: 4773 Rating: (123) |
New question published by AutoGen_905449 is split to a separate thread with the subject Valve control in STEP7. Best regards |
Follow us on