Industry Online Support
Technical Forum
3/5/2008 11:54 AM | |
Joined: 4/24/2006 Last visit: 9/24/2024 Posts: 8742 Rating: (1168) |
Hello no_nickname, Have you seen this faq: http://support.automation.siemens.com/WW/view/en/23802404 When you are using a PC-adapter, you cannot connect direct to panel. Because PC-adapter needs power from panel. You can try to use a PC-adapter connected to CPU-port and download to panel. (but like in faq mentioned, it's not supported) Best regards, Wizard |
3/5/2008 12:02 PM | |
Posts: 6 Rating: (0) |
So, do you think if i use a labtop with a com connexion it should work? thank you |
3/5/2008 1:08 PM | |
Posts: 220 Rating: (14) |
Hi, with a COM interface AND an RS232/MPI it will every time be luck if its work, thats one of the reasons this cable is not released for download a project to a panel.. Correct is the panel doesnt give enough power to run the Adapter. Serial in this case means RS232(USB)/PPI - Cable, see also http://support.automation.siemens.com/WW/view/en/19109408 regards Aranel |
3/5/2008 2:01 PM | |
Posts: 6 Rating: (0) |
Thank you guys, we are going to buy a usb host to host cable |
Follow us on