9/6/2006 4:34 PM | |
Posts: 7 Rating: (0) |
Hello Did you activateall alarm classesin the configuration of the alarm window? |
9/6/2006 4:45 PM | |
Posts: 13 Rating: (0) |
Yes I did. I configured everything as it should be. I have had a lot of problems with this panel. Am I missing a HotFix or a Service Pack?? |
9/8/2006 11:20 AM | |
Joined: 9/28/2005 Last visit: 12/14/2022 Posts: 414 Rating: (28) |
Hi, This communication should work from WinCC flexible 2004 SP1 + HSP1.1, according to FAQ http://support.automation.siemens.com/WW/view/en/14188898. Above that I've had customers who could put this panel into work as they wanted. Which bits are you using for these alarms? What happens if you set all these bits? Is other communication possible? Can you get an active counter value shown on the display? If you configure a button for setting a bit, does this work? At this moment I discovered a tiny difference between your version and mine, I'm using WinCC flexible Advanced 2005 SP1 HF4 (K1.1.1.4_1.2.0.1). This Hotfix 4 for WinCC flexible 2005 (Compact / Standard / Advanced) can be downloaded from http://support.automation.siemens.com/WW/view/en/22407633. According to the FAQ it is not necessary for 2005 Micro. |
Last edited by: Smurf at: 9/8/2006 11:21 AMSmurf |
|
Follow us on