Industry Online Support
Technical Forum
1/25/2008 4:57 PM | |
Posts: 33 Rating: (0) |
Hi myquestion is about print.I have a tp 270 10.İf I connect my computer-(tp270-10) with serial cable (IF2 PORT).Can I print alarm list?So like that : |
1/28/2008 5:21 PM | |
Joined: 5/8/2006 Last visit: 4/19/2024 Posts: 1085 Rating: (77) |
Hi, if you want to write an driver for that than you can use that. Why do you not use the USB port of the panel for the printer? You find more information about the TP270 and a printer in the chapter 4.3.4 of the manual. Link for the manual of the TP270: http://support.automation.siemens.com/WW/view/de/18796343/0/en If you want to connect a PC between the panel and the printer than you should use a TP177 because the panel has an OnBoard-Ethernet interface. Note: If you want to use an Ethernet printer you need an print server (e.g. PC). Bye |
Follow us on