4/10/2014 7:39 AM | |
Posts: 1299 Rating: (136)
|
Hello, this is a problem with your windows settings. see this link: http://support.automation.siemens.com/WW/view/de/90301561 K!ke |
4/15/2014 2:25 PM | |
Posts: 1299 Rating: (136)
|
Hello, this is also caused by the windows display settings: http://support.automation.siemens.com/WW/view/en/13899072 |
4/22/2014 4:54 PM | |
Posts: 1299 Rating: (136)
|
Hello, did you try what it looks like if you simulate the panel on the engineering pc? K!ke |
4/23/2014 3:42 AM | |
Joined: 1/14/2014 Last visit: 6/2/2024 Posts: 112 Rating: (1) |
Hi K!ke, Interestingly now when I simulate the panel in TIA (runtime) it shows up the same as it does on the actual TP700 panel. The problem is, it doesn't show up that way in WinCC when I actually create the layout. You can find examples of what I'm talking about attached. Thanks.
AttachmentUser Admin - WinCC V12.zip (181 Downloads) |
4/23/2014 8:40 AM | |
Posts: 1299 Rating: (136)
|
Hello, if you set dpi to 96 pt and the display size to 100% I don't know what should be wrong Maybe you should start a support request to solve this. It would be great if you share your solution afterwards. K!kr |