11/23/2019 11:23 AM | |
Joined: 12/27/2018 Last visit: 7/17/2023 Posts: 509 Rating: (41) |
1) refer Link I used to to make back up by using Service and commissioning command in TP700 control panel.Here you get back up option with license key.The HMI program will be backed up to external storage device.Also restore the backup files by options there. This method is easy.Actually no need prosave to do this activity. 2) I got same problem earlier.I have opened the original HMI program and tried to go online, then it worked.Also I have done license key authorization there. 3) Prosave back up is not editable. Error pic: Go to transfer settings in control panel and select the transfer settings to solve the issue. Refer below video |
Last edited by: JKV JAMES at: 11/23/2019 11:24:33Last edited by: JKV JAMES at: 11/23/2019 11:26:02Last edited by: JKV JAMES at: 11/23/2019 11:27:11Jinson James, P.Eng, BE, M.Tech (Power System),PGDM, MBA |
|
This contribution was helpful to1 thankful Users |
Follow us on