4/7/2016 1:26 PM | |
Posts: 107 Rating: (20) |
Did you set PG/PC interface on your laptop to be via Ethernet card ?? |
4/7/2016 2:06 PM | |
Posts: 17 Rating: (0) |
Hello, The MLFB it´s 6AV6 643-0CD01-1AX1 and v 1.2 Regards, |
4/7/2016 2:07 PM | |
Posts: 17 Rating: (0) |
Yes, The PG/PC it´s right (broadcom TCP/IP Activ) Regards, |
4/7/2016 2:15 PM | |
Posts: 17 Rating: (0) |
This is from the operator panel |
4/7/2016 2:22 PM | |
Joined: 5/12/2006 Last visit: 4/26/2024 Posts: 22231 Rating: (2980) |
and now a screen from the panel in the project and the data from this |
4/8/2016 9:40 AM | |
Posts: 17 Rating: (0) |
Good morning! Yes, this is my selection. Could be the versión of the MP? Regards, |
4/8/2016 12:09 PM | |||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Joined: 5/28/2008 Last visit: 4/15/2024 Posts: 4505 Rating: (835) |
Hello, And to Update the MP version or reset to factory setting you should use ONLY one of the following cables with character U for update / restore factory setting or with character D for update.
|
||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
Ayman Elotaify |
|||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||||
4/13/2016 1:59 PM | |
Posts: 17 Rating: (0) |
I can do ping to the MP panel |
4/13/2016 2:02 PM | |
Posts: 17 Rating: (0) |
MP transfer settings |
Follow us on