9/26/2017 8:11 AM | |
Joined: 7/9/2015 Last visit: 8/30/2024 Posts: 3943 Rating: (585) |
Hi, you can check also the following FAQ - it helps you to switch STL to LAD. Why can you not display an STL program in FBD or in LAD?Regards, Towome |
|
|
9/26/2017 11:42 AM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating: (1) |
hello Sir ALEX MOL thank you and here are the screenshots I really need you to convert me all to LADDER but there is a trick that I do not quite understand, is the call of the FC187 generates an instance DB every time in a LIST programming, if true, how to know the different instance DBs that have been created during each call of the FC187. Thank you for helping me and I am always online, it is really urgent AttachmentLIST TO LADDER.docx (234 Downloads) |
Last edited by: franckaay roy at: 9/26/2017 11:42:43 AM |
|
9/26/2017 2:39 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating: (1) |
thank you Mr. TOWOME for your help |
9/26/2017 5:05 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating: (1) |
thank you very much Mr. ALEX MOL but the problem is that M22.1 does not go to 1, it is always zero as the same block FC187 is called several times in the FC23 for SET or RESET either M22.0, M22.2 etc ... how to find out why M22.1 does not go to 1 because when I look at the FC187 view I do not see any value in #SPEED and as this same block handles the startup of M22.0, M22.1, M22.2 and other. I do not understand how M22.1 will go to start the machine. when a same block FC187 is called several times to turn on several outputs, how to see the operation of each output to know what is wrong and why an output does not activate, because I when I look I do not understand good here are still images being online, thank you for helping me.
AttachmentLIST TO LADDER.pdf (210 Downloads) |
9/27/2017 6:31 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating: (1) |
thank you very much Mr. ALEX MOL, I will try but the worry is that I'm new to the company and when I look at the SCADA, I do not see where I need to increment #speed and also when I ask the machinist he tells me he does not know how to increase it. I want to ask if I can create a variable table to force #speed to 40.50 etc to see the state that M22.1 will take. the DB10.DBW96 is used twice in the program. Here is the ZIP file of the machine program. it is in the project (EXTRUDER) that FC187 is found and it is in FC23 that it is called. it is in the project (LINE) that is the automatic operation of the machine: FC109 network10 and when I select the automatic mode it is the contact DB101.DBX4.1 which does not close so that the coil M159.7 is activated to be able to start the machine, thank you and I am always online. is that you can show me as a screenshot how I have to put ("//") to turn off network 50 to see what's going on in network 51 and also i want to know if it's a program that is written in LADDER or in LIST in TIA PORTAL or SIMATIC MANAGER and a call of the same block is made several times, how we do to see the values of the different networks where the block is called Attachment40084c_P.zip (152 Downloads) |
9/28/2017 7:31 PM | |
Joined: 2/10/2015 Last visit: 8/21/2024 Posts: 288 Rating: (1) |
for the SCADA of which I spoke, it is a computer that is connected to the PLC for the control of the machine |
Follow us on