9/24/2015 4:20 PM | |
Posts: 14 Rating: (0) |
Hi, I am trying to use a trend in a report but i cannot get the Trend Control object to work. I have looked all over but have not found any manuals or examples for how to configure trends in reports. i also need to set the end time and the begining time for the X-axis dynamicaly as well as change the date and time format. if i use the Print Provider.Picture i can get the trends but the resolutions of the picture is is to low (see attachement). If i could improve the resolution of this object it would solve my problems but i cannot find any way of doing it. AttachmentTrendReport.rar (222 Downloads) |
9/25/2015 11:57 AM | |
Posts: 14 Rating: (0) |
Hi, I tried using the Classic trend but i cant get the dynamics to work. the trend will only use the configuration from the "Assigning parameters" tab. I also need to change the date/time format to "yyyy-mm-dd hh.mm" and not use AM/PM. is there any way of doing this? I have attached the classic trend. AttachmentTrendControl (Classic).rar (185 Downloads) |
Follow us on